2024-09-30 3:58 AM
Hello everyone,
I'm experiencing issues with the "Write Multiple Blocks" command on the RF side using the ST25DV64KC.
I’ve tried using this command through the ST25 Android app, specifically using the "Send Custom Command" feature. Here’s how I configured the command:
Option Flag: Enabled
Addressed Mode: Enabled
Select Mode: Disabled
High Data Rate: Enabled
Format Extension: Disabled
"CMD" Code: 0x24
Data: 00 01 11 11 11 11 22 22 22 22
However, when I send this command, the Android app returns an "ERROR CMD" message.
I’ve also tried different configurations (e.g., disabling High Data Rate, using different data values, etc.), but I get the same result each time.
I want to note that the single block write command works perfectly and allows me to write one block at a time without any issues.
Does anyone know what might be causing this error?
Thanks in advance!
Solved! Go to Solution.
2024-09-30 4:44 AM
Hello,
Did you try to disable the Option flag?
I don't recommend using the option flag for this command as some smartphones may have timing issue when using this command with option flag set.
A general rule, I don't recommend using the option_flag=1 for any write-alike command. It is not necessary for the St25DV64KC and brings nothing interesting, it just slows down the response.
Best regards.
2024-09-30 4:44 AM
Hello,
Did you try to disable the Option flag?
I don't recommend using the option flag for this command as some smartphones may have timing issue when using this command with option flag set.
A general rule, I don't recommend using the option_flag=1 for any write-alike command. It is not necessary for the St25DV64KC and brings nothing interesting, it just slows down the response.
Best regards.
2024-10-01 12:07 AM
Hello!
Thank you a lot! I resolved the issue with your tips.
Best regards.