2017-12-19 02:03 PM
I'm using a M24LR64E-R and I can't seem to get the ST NFC Tap iPhone app to recognize it. I can get it to work with the M24LR-discovery board which has the M24LR04E-R on it.
I'm pretty sure I have a valid NDEF record on the M24LR64E-R. However, when I read both tags with the Android ST25 app, it lists 'NFC type V - ISO/IEC 15693' for the discovery board, but only lists 'ISO/IEC 15693' for my board. I have even tried saving the memory from the discovery board and dumping it on mine, with no luck.
Is it possible to read a M24LR64E-R with an iPhone?
#ios #nfc #m24lrSolved! Go to Solution.
2017-12-20 05:25 AM
Dear Brian,
Unfortunately, M24LR64E-R is not supported by iPhones. It is only supported on Android platforms.
As of today, iOS11 is not supporting NFC-V / ISO15693 tags with memories larger than 8Kbits.
Best regards,
2017-12-20 05:25 AM
Dear Brian,
Unfortunately, M24LR64E-R is not supported by iPhones. It is only supported on Android platforms.
As of today, iOS11 is not supporting NFC-V / ISO15693 tags with memories larger than 8Kbits.
Best regards,
2019-02-13 01:22 AM
@ST Community i have raised this issue on Apple Bug Reporter they have got back to me asking for more details. is there a technical person inside ST i could give as contact to Apple maybe this could be fixed in CoreNFC framework