2019-02-14 6:53 AM
Dear ST team,
I know that you can not provide Mifare Classic implementation for ST25R391x chip, but I am really having trouble on implementing it by myself. Could you please, provide any similar example, that I can use as a starting point? What I already did is selecting card using iso14443ASelect function and reading card info into iso14443AProximityCard_t structure. After that I am trying to perform authentication of memory block 0 using rfalTransceiveBlockingTxRx function, but I never receive anything back from card. Do I miss a step between these procedures? Do I use correct function or should I use another one for transmit/receive? Any help would be appreciated. Thanks in advance.
Best regards,
Van
Solved! Go to Solution.
2019-02-14 7:23 AM
Hi Van,
If it is really a Mifare Classic card (SAK 08) it should answer to an authenticate request.
Most transceives will need RFAL_TXRX_FLAGS_PAR_TX_NONE | RFAL_TXRX_FLAGS_CRC_TX_MANUAL | RFAL_TXRX_FLAGS_CRC_RX_KEEP | RFAL_TXRX_FLAGS_PAR_RX_KEEP and your own generated CRC and parity.
Regards, Ulysses
2019-02-14 7:23 AM
Hi Van,
If it is really a Mifare Classic card (SAK 08) it should answer to an authenticate request.
Most transceives will need RFAL_TXRX_FLAGS_PAR_TX_NONE | RFAL_TXRX_FLAGS_CRC_TX_MANUAL | RFAL_TXRX_FLAGS_CRC_RX_KEEP | RFAL_TXRX_FLAGS_PAR_RX_KEEP and your own generated CRC and parity.
Regards, Ulysses
2019-02-14 7:25 AM
Hi Ulysses,
Thanks for the answer, I will try this flags. I was using RFAL_TXRX_FLAGS_DEFAULT flags.
Best,
Van