2016-10-10 03:42 AM
Hello,
I am trying to create an application SW using M24LR-DISCOVERY using RF transceiver board to read devices containing M24LR dual eeprom, but I am struggling to get the documentation to implement functions like the M24LR-DISCOVERY SW has like auto-detect, read memory from - to.... etc. The only documentation I've found are AN3375 Application note and AN3163 Application note. Is there any docs explaining which function and which parameters I need to use to get any result. example: detect and read from EEPROM address 0x15 - CR95HFDLL_USBconnect() - CR95HFDll_SELECT() - CR95HFDll_SendRec() Thanks, SasaSolved! Go to Solution.
2016-10-17 08:12 AM
Hi,
there is an Application note explaining how to develop a software to drive CR95HF board : AN3954 and associated source code example, available on
:AN3954 :
Also available, source code examples (C & VB6) : Best regards ST customer supportHello,
I am trying to create an application SW using M24LR-DISCOVERY using RF transceiver board to read devices containing M24LR dual eeprom, but I am struggling to get the documentation to implement functions like the M24LR-DISCOVERY SW has like auto-detect, read memory from - to.... etc. The only documentation I've found are AN3375 Application note and AN3163 Application note. Is there any docs explaining which function and which parameters I need to use to get any result. example: detect and read from EEPROM address 0x15 - CR95HFDLL_USBconnect() - CR95HFDll_SELECT() - CR95HFDll_SendRec() Thanks, Sasa2016-10-17 08:12 AM
Hi,
there is an Application note explaining how to develop a software to drive CR95HF board : AN3954 and associated source code example, available on
:AN3954 :
Also available, source code examples (C & VB6) : Best regards ST customer supportHello,
I am trying to create an application SW using M24LR-DISCOVERY using RF transceiver board to read devices containing M24LR dual eeprom, but I am struggling to get the documentation to implement functions like the M24LR-DISCOVERY SW has like auto-detect, read memory from - to.... etc. The only documentation I've found are AN3375 Application note and AN3163 Application note. Is there any docs explaining which function and which parameters I need to use to get any result. example: detect and read from EEPROM address 0x15 - CR95HFDLL_USBconnect() - CR95HFDll_SELECT() - CR95HFDll_SendRec() Thanks, Sasa