2024-10-25 3:52 AM
Hello STM Community,
I'm currently working on a project involving the ST25DV04KC-IE8C3 NFC chip interfaced with the STM32L496ZG microcontroller. I've encountered an issue where the performance of the NFC chip deteriorates when a magnet is brought near the system, specifically related to the operation of a magnetic switch that generates interrupts.
I have attached a photo of the PCB layout for your reference. I would greatly appreciate any feedback on the design or suggestions on mitigating this issue!
Thank you for your assistance!
Solved! Go to Solution.
2024-10-25 7:10 AM
Hello,
NFC is based on magnetic coupling between the reader and the tag. The reader is emitting a magnetic field at 13.56MHz that is captured by the tag's antenna, creating current into the antenna. Having a magnet nearby may disturb the magnetic field emitted by the reader.
Does the issue appear when there is a reader communicating with the tag and a magnet is put close to the switch? Or do you have issues when there is no RF reader in front of the tag?
Best regards.
2024-10-25 7:10 AM
Hello,
NFC is based on magnetic coupling between the reader and the tag. The reader is emitting a magnetic field at 13.56MHz that is captured by the tag's antenna, creating current into the antenna. Having a magnet nearby may disturb the magnetic field emitted by the reader.
Does the issue appear when there is a reader communicating with the tag and a magnet is put close to the switch? Or do you have issues when there is no RF reader in front of the tag?
Best regards.