2020-12-26 6:11 PM
I have purchased "X-Nucleo-NFC03A1" NFC reader evaluation board. Can I use Arduino Uno to control the NFC board? and does anyone have a sample library?
Solved! Go to Solution.
2021-01-05 3:23 AM
Hi,
the X-NUCLEO-NFC03A1 library is currently compatible only with stm32duino boards. The job to make it compatible also with Arduino Uno should not so difficult because basically the board uses the standard APIs of Arduino framework. I suppose that there are some typedef and define to adjust in order to remove some errors that you can get with Arduino UNO target. Anyway, I'm not sure that Arduino UNO has enough flash and RAM memories to run the X-NUCLEO-NFC03A1 library.
Best Regards,
Carlo
2021-01-04 5:48 AM
Hi,
you can find a sample lib here https://github.com/stm32duino/X-NUCLEO-NFC03A1
there is also another library for Arduino. This is originally for the BM019 board but should run with X-NUCLEO-NFC03A1 with no or only little changes.
Rgds
BT
2021-01-04 2:21 PM
Thank you for your help, Brian.
I am using Arduino Uno R3 to control X-Nucleo-NFC03A1. I got the following error message while uploading the sample code in the library.
"WARNING: library X-NUCLEO-NFC03A1 claims to run on stm32 architecture(s) and may be incompatible with your current board which runs on avr architecture(s)"
I am wondering that I can use Arduino Uno for X-Nucleo-NFC03A1. or, should I use stm32duino board?
Regards,
JYP
2021-01-05 3:23 AM
Hi,
the X-NUCLEO-NFC03A1 library is currently compatible only with stm32duino boards. The job to make it compatible also with Arduino Uno should not so difficult because basically the board uses the standard APIs of Arduino framework. I suppose that there are some typedef and define to adjust in order to remove some errors that you can get with Arduino UNO target. Anyway, I'm not sure that Arduino UNO has enough flash and RAM memories to run the X-NUCLEO-NFC03A1 library.
Best Regards,
Carlo