cancel
Showing results for 
Search instead for 
Did you mean: 

Is there a provision to read temperature sensor value using SDK of ST25RU3993-EVAL board?

Lakshmikanth
Associate II

Using ST25RU3993, I was able to get only the On-chip RSSI value and EPC,PC values.

Is reading the temperature sensor value, implemented in the SDK?

If NO, How can i implement it??

The temperature Sensor which I am using is "RFM3200-AFR"(Gen2 compatible).

1 ACCEPTED SOLUTION

Accepted Solutions
Ulysses HERNIOSUS
ST Employee

Hi,

I guess this is the same request as st25ru3993eval-access-memory-bank-of-temperature-sensor.

We have all the required information and colleague of mine will provide an answer after this holiday period.

No need to double post.

Regards, Ulysses

View solution in original post

1 REPLY 1
Ulysses HERNIOSUS
ST Employee

Hi,

I guess this is the same request as st25ru3993eval-access-memory-bank-of-temperature-sensor.

We have all the required information and colleague of mine will provide an answer after this holiday period.

No need to double post.

Regards, Ulysses