2023-09-13 9:32 AM
Hi there,
I'm developing a board that features the ST25R3911B chip. At the moment I managed to integrate the module in order to read and write simple NTAGs (t2t), with plain text (both on demoboard X-NUCLEO-NFC05A1 and my custom board).
The next step is to interface with higher-level devices (smartphones) and I need to read and write custom APDUs based on standard ISO7816. I'm not familiar with that (and generally with NFC protocols).
Does somebody know how I can achieve that?
Thank you so much!
Solved! Go to Solution.
2023-09-14 5:21 AM
Hi,
just have a look at ST25 embedded NFC lib and its NDEF RW example: Reading/Writing NDEF on T4T is using ISO7816 APDUs on top of NFC Forum ISODEP/ISO14443-4 Data Link Layer / T=CL layer.
BR, Ulysses
2023-09-14 5:21 AM
Hi,
just have a look at ST25 embedded NFC lib and its NDEF RW example: Reading/Writing NDEF on T4T is using ISO7816 APDUs on top of NFC Forum ISODEP/ISO14443-4 Data Link Layer / T=CL layer.
BR, Ulysses
2023-09-14 6:03 AM
Hi Ulysses,
I didn't see that!
thanks so much, I will let you know
Best regards