2020-07-04 9:12 PM
can anyone can help you in this regard?
Solved! Go to Solution.
2020-07-07 1:08 AM
2020-07-07 1:27 AM
What are the values of Header Library path and Library search path into your build settings ?
2020-07-07 7:31 AM
2020-07-07 8:09 AM
Please, check value of Library Path into build setting, and verify that libST25SDK.a exists in NFCTap/st25sdklib
Let me know
2020-07-08 12:25 AM
2020-07-08 5:23 AM
Hi Vincent, Do you have any suggestion to fix this issue?
Issue: Command Ld failed with a nonzero exit code
2020-07-08 11:13 PM
sorry , I was on leave yesterday...
Sometimes , this issue happens in Xcode env for unknown reason..
Please, Try the following :
2020-07-13 6:46 AM
Hi Vincent,
Yes, Thanks for the advise.
we are able to compile & test the App.
Thanks,
Albert John
2020-07-20 11:23 PM
Hi Vincent
We are facing issue while writing "Multiple Blocks"
Facing error lie "Invalid Handle".
This error is coming up in the ST25 iOS App which is in Apple Store.
Do you have any suggestions to fix this issue?
Thanks,
Albert John
2020-07-20 11:33 PM
hi albert,
This is an error in buildtime or runtime ?
Please, could you give me the test case sequence in order to be able to reproduce issue ?
ex : select tag memory => Write => Write multiple block => @ start + Data to write...
I know that depending on tag type, or area configuration, you cannot write too much multiple blocks.
Let me know.
Br,