2019-02-19 02:01 AM
I have successfully read an epc tag, my next step is to issue the the Req_RN command. I hav set the RX lenthg register ready to receive 4 bytes of data and issue the Req_RN command. OIn the occasion that I do receive the expected 4 bytes of data they never seem to be a matching RN and CRC16. Can any one help?
Solved! Go to Solution.
2019-04-03 12:35 AM
Yes this is now fixed. It seemed to be a timing issue.
2019-04-03 12:32 AM
Hello Chris,
since in another thread your are already using the READ command I would assume that you have come by this problem already?
Cheers,
B
2019-04-03 12:35 AM
Yes this is now fixed. It seemed to be a timing issue.