cancel
Showing results for 
Search instead for 
Did you mean: 

Firmware of M24LR transceiver board _ Error occured during program operation!

ZMohd.7
Associate III

Hi,

I'm working with M24LR Discovery and I would like to Flash demonstration firmware of RF transceiver after erasing flash using STLINK/V2 utility.

I am able to erase the Flash but while I'm trying to Flash the .hex or Binary file, following error message displayed on Log window.

Unexpected error

Error occured during program operation!

below log is for your reference.

15:10:04 : ST-LINK SN : 50FF6D067788545417281567

15:10:04 : V2J34S7

15:10:04 : Connected via JTAG.

15:10:04 : JTAG Frequency = 140 KHz.

15:10:04 : Connection mode : Normal.

15:10:04 : Debug in Low Power mode enabled.

15:10:04 : Device ID:0x410 

15:10:04 : Device flash Size : 128KBytes

15:10:04 : Device family :STM32F10xx Medium-density

15:10:15 : Flash memory erased.

15:10:19 : ST-LINK SN : 50FF6D067788545417281567

15:10:19 : V2J34S7

15:10:19 : Connected via JTAG.

15:10:19 : JTAG Frequency = 140 KHz.

15:10:19 : Connection mode : Normal.

15:10:19 : Debug in Low Power mode enabled.

15:10:19 : Device ID:0x410 

15:10:19 : Device flash Size : 128KBytes

15:10:19 : Device family :STM32F10xx Medium-density

15:10:22 : Flash memory erased.

15:10:25 : [Demo.hex] opened successfully.

15:10:25 : [Demo.hex] checksum : 0x001F70E8 

15:10:27 : Unexpected error

15:10:27 : Error occured during program operation!

Thanks in Advance!!0693W000003QJWUQA4.png

1 ACCEPTED SOLUTION

Accepted Solutions
Berenice BENVEGUDA
ST Employee
1 REPLY 1
Berenice BENVEGUDA
ST Employee