cancel
Showing results for 
Search instead for 
Did you mean: 

Detect external NFC antenna connected to CR95HF.

Jignesh
Associate III

Hi,

We are using NFC reader IC: CR95HF using uart communication with our micro-controller.

We are using external antenna for antenna, Is there any way to detect NFC antenna is connected to CR95HF ?

Thank you in advance,

Jignesh Patel

1 ACCEPTED SOLUTION

Accepted Solutions
Brian TIDAL
ST Employee

Hi Jignesh,

Depending on your application, I would see several way for checking that the antenna is functional.

  1. use the Pollfield command and check the result code when the CR95HF is in the operating field of another reader. See §5.5 in the datasheet.
  2. use the TagDetection calibration procedure: when the antenna is disconnected/broken, the calibration value should be highly different from the one in nominal condition. See §5.9 in the datasheet.
  3. add a field detector (see https://www.youtube.com/watch?v=dTv4U5fotM0), switch on the field and check that the field is present.

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3
Brian TIDAL
ST Employee

Hi,

can you elaborate on your need:

  • Is it for production testing?
  • Is it for integrity testing during lifetime of your product?
  • etc.

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Jignesh
Associate III

Hi Brian TIDAL,

It is for integration of system check during lifetime of product.

Regards,

Jignesh Patel

Brian TIDAL
ST Employee

Hi Jignesh,

Depending on your application, I would see several way for checking that the antenna is functional.

  1. use the Pollfield command and check the result code when the CR95HF is in the operating field of another reader. See §5.5 in the datasheet.
  2. use the TagDetection calibration procedure: when the antenna is disconnected/broken, the calibration value should be highly different from the one in nominal condition. See §5.9 in the datasheet.
  3. add a field detector (see https://www.youtube.com/watch?v=dTv4U5fotM0), switch on the field and check that the field is present.

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.