Hi,We are using NFC reader IC: CR95HF using uart communication with our micro-controller.We are using external antenna for antenna, Is there any way to detect NFC antenna is connected to CR95HF ?Thank you in advance,Jignesh Patel
Hi,We are using NFC tag IC ST25DV04K using I2C communication with our micro-controller.Is there any way to detect, if the NFC antenna is connected or not to ST25DV04K using any I2C command?Thank you in advance,Jignesh Patel
We have ordered ST25-TAG-BAG-U. I want to write a password protected data on ST25TV02K tag from it.I have downloaded ST25 anroid application to communication with tag.Using Application I can read & write NDEF text on tag using ISO/IEC 15693 protocol ...
Hi,We are using ST25DV04K dynamic tag with internal taoglas antenna FXR.07.A with ISO15693 protocol in our product. We are hardly getting 4cm distance with CR95HF reader. We would like to increase distance upto ~9cm. With same reader we can get 7-8c...
I have successfully communicated with CR95HF using usb to uart bridge using uart communication. I can read my nfc tag(BL654- type 2) UID using command send from terminal by selecting ISO14443-A protocol.But I have problem with reading data from tag h...
@JL. Lebon_O @Brian TIDAL_O I have checked using EH_CTRL_Dyn register by reading bit 2 FIELD_ON. it detect the RF field if i take ST25DV04K near reader.I want to detect antenna connected it self to ST25DV04K without reader.Thank you,Jignesh Pate...