cancel
Showing results for 
Search instead for 
Did you mean: 

Demo CR95HF-A ISO 15963 max range

pieretti
Associate II
Posted on January 23, 2014 at 11:23

Hi,

I'm trying to achieve the maximum reading range from my demoboard CR95HF-A with a ISO 15693 tag (LRi2K). Until now I've obtained best results with modulation-index 10% and gain 34dB by writing 0x50 to ARC_B register: only 5 cm.

Can I improve this result? How Can I increse the antenna current?

Thanks in advance.

#range #lri2k #lri2k #lri2k #lri2k #lri2k #demo-cr95hf-a #cr95hf-firmware #cr95hf
1 ACCEPTED SOLUTION

Accepted Solutions
Anais GALLIGANI
Senior II
Posted on March 04, 2014 at 17:34

Hello,

the FW can be find in the following link :

http://www.st.com/web/en/catalog/tools/FM116/SC1444/PF253360

#

and then in tab ''tools & software''

http://www.st.com/web/en/catalog/tools/PF257512

Have a nice day,

ST NFC/RFID Dynamic tag e2e support

View solution in original post

13 REPLIES 13
Anais GALLIGANI
Senior II
Posted on January 23, 2014 at 14:35

Hi Andrea,

Thanks for the interest in our line of product,

In order to help you further, I have a bundle of questions, sorry about that,

- What is the size of your tag? 

- Is the reader : DEMO-CR95HF-A  

MB1054A ?

- What is the answer to IDN ? 

Thanks,

ST NFC/RFID Dynamic support

Hi,

I'm trying to achieve the maximum reading range from my demoboard CR95HF-A with a ISO 15693 tag (LRi2K). Until now I've obtained best results with modulation-index 10% and gain 34dB by writing 0x50 to ARC_B register: only 5 cm.

Can I improve this result? How Can I increse the antenna current?

Thanks in advance.
pieretti
Associate II
Posted on January 24, 2014 at 09:26

First of all, thank you for your quick reply.

These are the answers:

- What is the size of your tag? I'm using a

http://www.st.com/st-web-ui/static/active/en/resource/technical/document/datasheet/CD00092187.pdf

2x3 mm2 inside a card: it came with the demoboard.

- Is the reader : DEMO-CR95HF-A   MB1054A ?

http://www.promelec.ru/pdf/DEMO-CR95HF-A.pdf

- What is the answer to IDN ? NFC FS2JAST0
Anais GALLIGANI
Senior II
Posted on January 24, 2014 at 16:22

What is the size of the tag's antenna? (sorry my question was confusing)

You have an old eval board, I suggest you to get a M24LR-discovery. Several options are possible :

1. buy it form distributors

2. You can request it to your ST 's sales.

  1. If you want you can contact me through moderator 's case of this forum.  Or let me your email.

     

pieretti
Associate II
Posted on January 27, 2014 at 14:27

The tag is inside a card: I don't know the real antenna size.

Which antenna size is recommended to achieve the best range with my demo board?
Anais GALLIGANI
Senior II
Posted on January 28, 2014 at 09:18

Hello Andrea,

Just to be sure, might you send a picture of the tag please?

thanks

Anais GALLIGANI
Senior II
Posted on January 28, 2014 at 11:39

Also if it is a ISO Tag embedded in the card,

Read range should be more like 8 cm.

Have you ordered a new evaluation kit?

pieretti
Associate II
Posted on January 28, 2014 at 15:58

0690X00000602oMQAQ.jpg

0690X00000602oHQAQ.jpg

Hello,

these are the picture you requested.

For this card, which are the best CR95HF settings to achieve the longest working range?

Which are the differences between my CR95HF demoboard and M24LR transceiverboard?

Thanks for your support

Anais GALLIGANI
Senior II
Posted on January 29, 2014 at 11:45

Ciao Andrea,

Yes, with the tag you got, read range is more around 8 cm. 

Difference betweend M24LR RF tranceiver board and DEMO-CR95HF-A , 

- EMI filter is present on the RF tranceiver board , http://www.st.com/st-web-ui/static/active/en/resource/technical/document/application_note/DM00089926.pdf

- better matching impedance, about that , there is an application note, http://www.st.com/st-web-ui/static/active/en/resource/technical/document/application_note/DM00027198.pdf

I hope you get better result with the board, let us know :)

Have a nice day,

ST NFC/RFID dynamic support

pieretti
Associate II
Posted on February 11, 2014 at 12:42

I've ordered the new Demoboard: I'll try my tests with this new hardware.

Thanks