2018-09-24 2:38 AM
We've built several prototypes of an IoT device that uses the CR95HF to detect the presence of 14443A tags and read their UID. The devices work fine for days/weeks, until eventually no data is received from the CR95HF UART.
To work around the issue we've implemented sending ECHO (0x55) in a loop which sometimes brings the CR95HF back to life (after minutes/hours of echoes). Often the only way out is to power cycle the CR95HF which unfortunately is not a solution, as end users will have to pull the battery to achieve that.
This issue currently prevents us from going into manufacturing.
Is there a way to reset the CR95HF UART communication without power cycling it?
2018-10-02 7:57 AM
Hello ooswald,
1st what are the settings of the CR95HF how it is configured and what are the wake up sources?
Then:
Can you provide more information on your error ?
Do you have a trace that shows the blocking point?
Does the UART communication broken when the issue is coming? or it is a RF communication issue?
Do you know how many echo command have been sent to go back to life?
Thank for your feedbacks
PB
2019-03-11 9:31 AM
Hi ooswald,
did you found the solution how to reset the CR95HF without power cycle?
Thank you