2019-12-10 4:07 AM
Solved! Go to Solution.
2019-12-11 4:54 AM
Hi,
an Arduino support is provided for X-NUCLEO-NFC03A1 ST25R95/CR95HF reader (see https://github.com/stm32duino/X-NUCLEO-NFC03A1). As far as I know, X-NUCLEO-NFC05A1 is not supported in Arduino environment. X-CUBE-NFC5 provides support for IAR Embedded Workbench for ARM, Keil Microcontroller Development Kit (MDK-ARM), and System Workbench for STM32 (SW4STM32).
Rgds
BT
2019-12-10 8:26 AM
Hi,
The ST Zio connector of the STM32 Nucleo-144 boards extends the Arduino™ Uno V3 connectivity, As explain in the STM32 Nucleo-144 boards User Manual (UM1974) §6.14, . most shields designed for Arduino Uno V3 can fit to the STM32 Nucleo-144 board. See §6.14 for details about hardware configuration of Nucleo-144 for the proper support of such shields.
See also "Having trouble with X-Nucleo-NFC03A1 and Nucleo-F413ZH" for similar question for support of X-NUCLEO-NFC03A1 with NUCLEO-F413ZH STM32 Nucleo-144 development board.
Make sure to make the proper pin assignment configuration. I would recommend to use STM32CubeMX for the pin assignment and the pin configuration.
For example with NUCLEO-F413ZH:
PA5 -- SPI1-SCLK
PA6 -- SPI1_MISO
PA7 -- SPI1_MOSI
PD14 -- SPI1_CS
PA3 -- IRQ_3911
PC0 -- LED_F
PC3 -- LED_B
PC1 -- LED_A
PF13 -- LED_FIELD
PE11 -- LED_V
PF14 -- LED_AP2P
Rgds
BT
2019-12-10 9:12 AM
Hi Brian, @Brian TIDAL_O
the OP probably expects that once the pinout is Arduino-ish, he/she would be able to program the board in the Arduino environment.
Is there such option?
JW
@YKim.2417 please change your username to a normal nick.
2019-12-11 4:54 AM
Hi,
an Arduino support is provided for X-NUCLEO-NFC03A1 ST25R95/CR95HF reader (see https://github.com/stm32duino/X-NUCLEO-NFC03A1). As far as I know, X-NUCLEO-NFC05A1 is not supported in Arduino environment. X-CUBE-NFC5 provides support for IAR Embedded Workbench for ARM, Keil Microcontroller Development Kit (MDK-ARM), and System Workbench for STM32 (SW4STM32).
Rgds
BT