cancel
Showing results for 
Search instead for 
Did you mean: 

ST25R3911B-DISCO compliant tags

NPeze.2138
Associate

I would like to find out if the eval board ST25R3911B-DISCO will be able to read the Avery Dennison RF700048 HF tag, which uses the NXP ICODE SLIX chip.

Thanks,

Narek

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Brian TIDAL
ST Employee

Hi ,

the ST25R3911B-DISCO Discovery kit for ST25R3911B can be operated as an ISO15693 reader thus the memory of the aforementioned tags can be read using the READ SINGLE BLOCK command as defined in ISO/IEC 15693-3.

On PC side, you can use either the ST25R3911B Discovery GUI (STSW-ST25R001) or the ST25PC-NFC Windows® PC software (STSW-ST25PC001).

Feel free to share more details about your application.

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Brian TIDAL
ST Employee

Hi ,

the ST25R3911B-DISCO Discovery kit for ST25R3911B can be operated as an ISO15693 reader thus the memory of the aforementioned tags can be read using the READ SINGLE BLOCK command as defined in ISO/IEC 15693-3.

On PC side, you can use either the ST25R3911B Discovery GUI (STSW-ST25R001) or the ST25PC-NFC Windows® PC software (STSW-ST25PC001).

Feel free to share more details about your application.

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.