cancel
Showing results for 
Search instead for 
Did you mean: 

Using hardware based wake-up in combination with the automatic antenna tuning feature is not recommended. I like to use both what should I do. And what is the card read range with this device

FTajb.1
Associate
 
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2

I guess you'd read all the docs, review all the code, and then own the dev/debug task to make it ​work.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Brian TIDAL
ST Employee

Hi,

can you provide more information about your request:

  • which ST25 device, what is your HW setup, custom board or ST board, etc.
  • FW setup, etc
  • what is your application

Thanks

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.