2024-06-24 2:57 AM
dear ST:
Why STSVAL-L99615C- can_not_connec to_GUI?
I can use tera toem connect to ST, But could not connect to GUI ?
I attached a ppt to descript this situation;
My email: 51296211@qq.com
Solved! Go to Solution.
2024-06-27 5:55 AM
Dear,
It is possible that you did not flash the right binary (present in the STSW-L99615C package), but instead you kept a binary from the STSW-L9961BMS package, the one that provides for the use of Tera Term.
This is why you are able to connect with Tera Term but have a communication error with the GUI software.
Let me know if you can solve it with this suggestion.
Best Regards
2024-06-27 5:55 AM
Dear,
It is possible that you did not flash the right binary (present in the STSW-L99615C package), but instead you kept a binary from the STSW-L9961BMS package, the one that provides for the use of Tera Term.
This is why you are able to connect with Tera Term but have a communication error with the GUI software.
Let me know if you can solve it with this suggestion.
Best Regards
2024-06-27 7:19 AM
Dear GS98:
It works well right now!
the GUI can communicate with STSVAL-L99615C now!
thanks for your kindly reply!
2024-06-27 7:21 AM
Dear,
I'm happy my suggestion was useful.
Best Regards