cancel
Showing results for 
Search instead for 
Did you mean: 

Where is it?

raddatzj
Associate II
Posted on July 23, 2009 at 13:48

Where is it?

3 REPLIES 3
raddatzj
Associate II
Posted on May 17, 2011 at 10:16

Hello,

I'd like to ask where I can download the FOC library for the STM32?

I used to download it at the STM32 main site but it seems to be gone?

I can only find the FOC Generator tool for Windows which is generating the necessary header files.

Are you doing a redesign or adaption to the new CMSIS compliant standard peripheral library?

Thanks a lot in advance and best regards

Jan

stello
Associate II
Posted on May 17, 2011 at 10:16

Hello Raddatzj,

normally the library is included in the STM32 MC Kit (I'm not sure it was published on internet). Did you buy one?

Regards,

Billino

raddatzj
Associate II
Posted on May 17, 2011 at 10:16

Hello Billino,

yes we've bought two of the MC Kits.

I got 2CD's within the boxes so I do have the FOC Software.

But! I used to download the newest versin of the library from your website and now the link seems gone! I was wondering if you are busy porting it to the new CMSIS compliant standard peripheral library and therefore removed the link?

I would be really glad if you could give me an info if there will be an updated version of the FOC software :)!

Thanks a lot in advance!

Best regards

Jan