2009-07-23 04:48 AM
2011-05-17 01:16 AM
Hello,
I'd like to ask where I can download the FOC library for the STM32? I used to download it at the STM32 main site but it seems to be gone? I can only find the FOC Generator tool for Windows which is generating the necessary header files. Are you doing a redesign or adaption to the new CMSIS compliant standard peripheral library? Thanks a lot in advance and best regards Jan2011-05-17 01:16 AM
Hello Raddatzj,
normally the library is included in the STM32 MC Kit (I'm not sure it was published on internet). Did you buy one? Regards, Billino2011-05-17 01:16 AM
Hello Billino,
yes we've bought two of the MC Kits. I got 2CD's within the boxes so I do have the FOC Software. But! I used to download the newest versin of the library from your website and now the link seems gone! I was wondering if you are busy porting it to the new CMSIS compliant standard peripheral library and therefore removed the link? I would be really glad if you could give me an info if there will be an updated version of the FOC software :)! Thanks a lot in advance! Best regards Jan