cancel
Showing results for 
Search instead for 
Did you mean: 

What is the maximum switching frequency of PWD13F60?

Arju
Associate
 
1 REPLY 1
Cristiana SCARAMEL
ST Employee

​The maximum switching frequency depends on application requirements, for example from the high voltage bus value, load current, load type and switching method (hard- or soft-switching).

Primarly, the switching frequency is limited by the switching losses (heat dissipation). You can estimate the maximum frequency, using your application requirements and the MOSFET characteristics reported in the PWD13F60 datasheet at page 10.

If you feel a post has answered your question, please click "Accept as Solution"