2019-03-05 9:18 PM
In the March 2015 datasheet it says that the hex reset value for the config register is 2C88. When I try this on my actual devices (4 of them) I get back 2C08. Based on the value this means that the OC_SD bit is set to 0 - Bridges do not shut down (page 56)
Is the correct value 2C08? Is there an error in the datasheet?
2019-03-07 5:58 AM
Solved my problem. The SPI mode in my code was wrong, as such the first bit of every byte transaction was being lost.