2024-01-31 03:54 AM
Hello
Since the VN920D-B5 chip is not available, I am looking for a replacement. I am looking for another system with similar parameters.
Please help me.
Solved! Go to Solution.
2024-02-01 11:32 AM
First of all, it must be mentioned here that the VN920D-B5 as well as the VN920-B5 has long been obsolete and the VN920B5TR-E is already on NRND.
However, as you have already discovered yourself: the STATUS pin on the discontinued VN920D-B5 was digital, while the CURRENT SENSE pin on the VN920B5TR-E (and the discontinued VN920-B5) is analogue, which is why one cannot replace the other without hardware and software changes.
Ah, and in case you're wondering what you can replace the VN920D-B5 with: I'm really sorry but I'm not aware of any alternative device.
Does it answer your question?
Regards
/Peter
2024-01-31 08:36 AM
Hello Pietia
If you mean VN920B5-E SINGLE CHANNEL HIGH SIDE SOLID STATE RELAY
the product is available.
https://www.st.com/en/automotive-analog-and-power/vn920b5-e.html
regards.
Elena
2024-02-01 12:35 AM - edited 2024-02-01 01:29 AM
VN920D-B5 - pin status digital
VN920-B5 - pin sense analog
Can I use VN920 instead of VN920D?
2024-02-01 11:32 AM
First of all, it must be mentioned here that the VN920D-B5 as well as the VN920-B5 has long been obsolete and the VN920B5TR-E is already on NRND.
However, as you have already discovered yourself: the STATUS pin on the discontinued VN920D-B5 was digital, while the CURRENT SENSE pin on the VN920B5TR-E (and the discontinued VN920-B5) is analogue, which is why one cannot replace the other without hardware and software changes.
Ah, and in case you're wondering what you can replace the VN920D-B5 with: I'm really sorry but I'm not aware of any alternative device.
Does it answer your question?
Regards
/Peter
2024-04-18 06:06 AM
Thanks for the answers.