cancel
Showing results for 
Search instead for 
Did you mean: 

VN5T016AH-E

bestyeng
Associate II

Hi all.
I would like to use the VN5T016AH-E high-side driver and I have some questions.
*Are there 8V in the CS pin under fault conditions?
*Can it measure max 4.2A with a K about 4240? Why do you specify 4V in the datasheet without knowing the value of the Rsense resistor?
*If I don't need latch-off option, is there an autorestart mode after a fault condition?

Many thanks.

bestyeng_0-1737207651002.png

 



0 REPLIES 0