‎2022-12-06 8:26 PM
Please help to share any docs showing date code in the top marking for the part number VN5T006ASPTR-E. The marking "209" denotes DC 2209 whist marking 101 denotes DC 2101. Please refer to attached photo for reference. Thank
‎2022-12-08 12:32 PM
The date codes are to be interpreted as always: YWW, which also applies to the VN5T006ASPTR-E, which has the component marking VN5T006A.
Since VN5T006ASPTR-E was launched in 2012, the examples should be read as:
Regards
/Peter
‎2022-12-14 10:50 PM
Dear Peter,
Thank you so much for the reply. I have a follow up question on this.
Kindly confirm if the highlighted in the photo marking code 9912B & 9908U are lot codes.
Thanks.
‎2022-12-15 8:22 AM
These codes 9912B and 990BU are no lot codes, but internal codes for production sites.
Regards
/Peter