cancel
Showing results for 
Search instead for 
Did you mean: 

VN5T006ASPTR-E Date Code

igamoso
Associate III

Please help to share any docs showing date code in the top marking for the part number VN5T006ASPTR-E. The marking "209" denotes DC 2209 whist marking 101 denotes DC 2101. Please refer to attached photo for reference. Thank

3 REPLIES 3
Peter BENSCH
ST Employee

The date codes are to be interpreted as always: YWW, which also applies to the VN5T006ASPTR-E, which has the component marking VN5T006A.

Since VN5T006ASPTR-E was launched in 2012, the examples should be read as:

  • 209 = 2012 or 2022, week 9
  • 101 = 2021, week 1

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
igamoso
Associate III

Dear Peter,

Thank you so much for the reply. I have a follow up question on this.

Kindly confirm if the highlighted in the photo marking code 9912B & 9908U are lot codes.

Thanks.

0693W00000WL4PPQA1.png

Peter BENSCH
ST Employee

These codes 9912B and 990BU are no lot codes, but internal codes for production sites.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.