2021-05-05 1:02 AM
Hi,
I'm planning to use STEF01 as a high-side switch plus an external MOSFET for blocking inverse current from load. Is this feasible or I would be wrong?
gaston
Solved! Go to Solution.
2021-05-05 8:11 AM
If you need more than 2.4A (until then the IPS160HF would be the better solution, also because it is considerably faster) and you are satisfied with the switch-on time (min 3ms), this should be possible. However, keep an eye to the maximum input voltage.
Regards
/Peter
2021-05-05 8:11 AM
If you need more than 2.4A (until then the IPS160HF would be the better solution, also because it is considerably faster) and you are satisfied with the switch-on time (min 3ms), this should be possible. However, keep an eye to the maximum input voltage.
Regards
/Peter
2021-05-05 8:27 AM
Hi Peter,
Understood. The problem is IPS160HF does not have the option for Reverse Current Blocking.
I'm basically looking for an alternative part to MP5016H but in my application the switching times are not so critical. I think STEF01 can be a good one. Thanks!
regards,
gaston