cancel
Showing results for 
Search instead for 
Did you mean: 

B-g431b-esc1 vs steval-esc001v1

Hannibal
Associate

Hello all,

I would like to understand the key differences between the two controllers and which one would better suit my needs.

​I want to precisely control the speed of two sensorless bldc motors, keeping them in sync regardless of the load each of those is experiencing.

Thanks, regards

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Dario CUCCHI
ST Employee

Hi @Hannibal​  and welcome to the ST Community !

Both boards operate with a battery pack from 3S to 6S Li-Po batteries (typical from 11.1V to 22.2V).

The peak current of the ESC001V1 is 30A, for the B-G431B-ESC1 it is 40A.

The B-G431B-ESC1 is more compact and uses the STM32G431 microcontroller; the  ESC001V1 uses the STM32F303 microcontroller.

The B-G431B-ESC1 has an embedded ST-LINK, useful for programming and debugging your application.

Both the evaluation boards can manage one motor; if you want to synchronize them, you have to use some external common signals, or use a central unit (for example the STEVAL-FCU001V1).

Here the link at user manual of the two boards for more information:

Have a nice day !