2017-11-19 02:24 AM - last edited on 2023-08-31 12:01 AM by Peter BENSCH
Posted on November 19, 2017 at 11:24
Hi!
I collect a three-phase control circuit (6kW).
I want to use BTA16 (Snubberless and standard Triacs)
Whether correctly I understand, that for type Standard it is necessary to include in parallel TVS a diode. And for the Snubberless TVS type, the diode will be superfluous (because it is already built in)?
Thank you. Sorry for my english.
#triac #tvs #ac-motor-control
2017-11-21 02:04 AM
Hello Rafil,
In both cases - Standard and Snubberless - no need of any TVS diode in parrallel.
Standard type is a four quadrants Triac (see application note AN4363 about 'How to select the Triac, ACS, or ACST that fits your application', section 3).
Snubberless Triac is a three quadrants Triac (No QIV operation), but with improved immunity to dV/dt and turn-off commutation.
Let me know if you need more details,
Benoit
2017-11-21 02:05 PM
Hi
Benoit!
Thanks for answering.
I got acquainted with AN4363 (Figure 9. Triac overvoltage protection by MOV (a) or Transil (b)). I want to apply the protection scheme Figure 9 (c) for my application.
Also, I got acquainted with AN1966 (TRIAC overvoltage protection using a TransilTM), described for protection using a TVS diode, instead of the Snubberless circuit.
Do you propose, with the Snubberless type, to abandon the protective circuit? And with the Standard type, use protection.
Maybe I do not understand something correctly.
2017-11-24 01:30 AM
Hi Rafil,
Regarding protection aginst voltage surges, no difference between Standard and Snuberless (only differences on quadrants, immunity and turn-off commutation as explained).
For the protective circuit against overvoltage surges, two ways:
- Implement a Transil between A2 and G to trigger the Triac when the surge voltage reaches the Transil breakover voltage (VBO). You are right, the AN1966 is a good start to design this circuit. Note that in this case the Triac must absorb the induced overcurrent.
- Use a MOV in parallel of the Triac (between A1 and A2), to clamp the voltage surge below the maximum voltage the Triac can sustain in non-repetitive (VDSM / VRSM parameter). For example, a 800 V Triac can sustain a maximum of VDSM = 900 V. Example of a MOV could be S14K420 (need to withstand your 3-phase voltage).
Let me know if you need more details on both solutions,
BR
Benoit