Skip to main content
jumman_JHINGA
Senior III
April 8, 2025
Question

'Vector Rendering' & 'Video Decoding' Not visible in TouchGFX settings of STM32H747I-Disco board

  • April 8, 2025
  • 2 replies
  • 1006 views

Hello Friends!

Im trying to configure TouchGFX manually on STM32H747I-Discovery board. Im using CubeMX version 6.14.0, after selecting TouchGFX for Cortex-M7 'Vector Rendering' & 'Video Decoding' options are not getting visible.

TouchGFX Manual ConfigurationTouchGFX Manual Configurationbut on other hand if im generating project through TouchGFX Designer and checking ioc file then these options are visible there.

TouchGFX Designer generated ConfigurationTouchGFX Designer generated Configuration

 i compared both project's ioc files i didnt get any diffrence.. is there any hidden setting do i have to enable for this isse? 

@Osman SOYKURT  @mƎALLEm  

 
 
This topic has been closed for replies.

2 replies

jumman_JHINGA
Senior III
April 11, 2025

Is anyone knows this isse?

 
ST Employee
April 11, 2025

Hello @jumman_JHINGA,

First, please do not mention members when you ask a question.
I tried on my side and I dont have this issue with a project made from scratch in CubeMx, also follow this tutorial 8. Hardware acceleration | TouchGFX Documentation to configure dma2D (for video hardware decoding).

BR,

Louis BOUDOST Software Engineer | TouchGFX