2019-12-09 03:17 AM
I am using stall detection when stepper motor enter under force. but temperature affact detection system. I am using same force in same system but stall detection feedback is different position in different temperature. I need to find force position. How can I solve this problem.
B.Regards.
Ahmet.
2020-01-09 03:27 AM
If I understand the topic, you are trying to evaluate the motor in overload condition, in particular which is the "torque threshold" that cause a motor stall.
The L6470 stall detection feature is designed to detect a motor stall condition. In this case the motor is not delivering torque.
It is not designed to sense a motor torque.
You can find more details on the sensorless stall detection system and how to work in the AN4241 at page 14.