cancel
Showing results for 
Search instead for 
Did you mean: 

Supply Voltage L6229Q

mikemike9147
Associate
Posted on February 22, 2015 at 23:56

Hi,

I am using the BLDC driver -L6229Q. I can see that the recommended operating conditions for the supply voltage is between 8 to 52 V.

What are the effects of supplying a lower voltage 6V? or 7V? 

After testing it I have't seen any difference in the results.

P.S - Is there a similar driver that can work with those supply voltages?

Thanks

0 REPLIES 0