2024-07-22 11:29 PM - edited 2024-07-22 11:33 PM
Hi all,
I am designing the custom wireless charging receiver using the STWLC38JRM chip
Currently, when I put the circuit on the wireless charging pad (Qi standard), I notice that the STWLC38JRM chip does not output 5V at the VOUT pin.
Below is the schematic, I copied all the things from the STDES-WLC38WA board, the coil part number is 760308101219 but the circuit does not work, the only thing that worked is the I2C communication, when I supply 5V to the VOUT pin, I was able to communicate and read ID chip.
and Below the schematic is the scope that I captured when put the circuit on the wireless charger pad
Red is AC1, green is AC2, yellow is VRECT, and blue is VOUT
I see the VOUT is still 0V and the AC1, AC2, and VRECT waveforms look like wrong.
Currently, I don't use the temperature sensor NTC so I designed a 100k resistor pull-down and 100k pull-up to VAA at NTC (F1 pin).
Can you guys help me fix this issue?
Thank you so much
2024-07-23 2:17 AM
Hi Sir
May i ask what is the application?
seems you follow our STDES-WLC38WA design. Please follow below link:
coil 760308101219 is 11.8 uh, based on https://www.we-online.com/components/products/datasheet/760308101219.pdf.
From your sch C tank is 247nF, seem right
From your waveform, Vrect send some ASK packet and then drop power, seems TX CEP timeout.
2024-07-23 2:44 AM
Hi @willzhou,
My application is a small wearable device
I copied all the schematics of the STDES-WLC38WA design, but my circuit does not work.
I think the schematic is correct.
I tried with another wireless charger pad but it still did not work.
With the above waveforms, what should I do next?
Thank you
2024-07-23 3:48 AM
HI
STDES-WLC38WA design work with STDES-WBC86WTX, and coils is smaller.
But you use TX with standard coils,
I suggest you modify COMA/COMB Cap value, make it larger, currently your sch COMA Cap 22nF and COMB Cap 10nF, suggest to modify to COMA Cap 47nF and COMB Cap 22nF
2024-07-24 12:13 AM
Hi @willzhou,
Below is the scope after I modify the 2 capacitors COMA from 22nF to 47nF and 2 capacitors COMB from 10nF to 22nF, it still does not work.
What should I do next? Should I continue to increase the capacitor value?
Also, I attached the image of my wireless charger pad that I am using, this pad can charge my iPhone XS Max
Thank you
Best regards
Hiep Le
2024-07-24 5:32 AM
HI
Do you have qi-sniffer, seems TX Control error timeout, just want to make sure.
Also can you use some TX what can see detail logs, for example STWBC2.
May i know what is the volume of application, and i can find local or related FAE to support you?
2024-07-24 5:55 AM
Hi @willzhou,
I don't have Qi-sniffer
This is the first time I have designed this STWLC38 chip and I don't have experience in this field.
My customer plans to produce 10,000 devices for this application
I am living and working in Vietnam, if you have any FAE, please help me
Or if you have any suggestions, please let me know, I will follow your guide, I need to debug and fix this issue ASAP.
Thank you so much
Best regards
Hiep Le
2024-07-24 6:10 AM
2024-07-24 6:23 AM
Hi @willzhou
Below is my custom PCB,
How can I use these firmware files?
Does the MCU need to communicate with the STWLC38 chip to enable the chip?
I think when placing the circuit in the TX charger, it will need to power up first, then the MCU can communicate and configure the STWLC38 chip. According to the current status, the STWLC38 chip has not been powered-up yet, so how can we use firmware to communicate with the STWLC38 chip?
2024-07-24 6:58 AM
Hi
Please follow this link, it have the answers.
https://community.st.com/t5/power-management/wireless-charging-solution-wiki/td-p/684177