cancel
Showing results for 
Search instead for 
Did you mean: 

STWBC2-HP and STWLC99: output only reaches 0.8A - expecting 5A

Fengji
Associate II

I am using STWBC2-HP and STWLC99 for development. The output voltage at the receiver end is set to 10V, and the current limit at the transmitter end is set to 5A. However, the actual current at the transmitter end can only reach a maximum of 0.8A, and I do not know why.

13 REPLIES 13

00234252

Didier HERROUIN
ST Employee

Hello,

I was able to find out the case 00234252, but as I am part of EMEA region, the request should be supported by my Asia-Pacific region colleagues.


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

So how can I get help?

Didier HERROUIN
ST Employee

Your case is opened in ST database, so a colleague of mine should take your point (you have nothing else to do).

By the way, you can start checking the STWBC2-HP input power supply (STWBC2-HP eval kit is supposed to be supplied by a USB-C charger): if you set the Rx Vout to 10V, the STWBC2-HP should adapt its input voltage to higher voltage (9V or 12V most probably). This input voltage is displayed by the GUI.


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.