2024-10-31 12:20 AM - edited 2024-10-31 12:23 AM
I have the following situation:
I have a custom PCB with a 4 port HUB ic on it (TUSB8041IRGCR). The UFP of the hub is connected to my phone and there are 4 DFP.
My phone negotiates with the PD controller via CC lines about what voltage it wants when phone is connected. The datalines of the usb port go to the hub. The thing is that the phone does not see the hub. If i completely ignore the USB PD negotiation and connect the UFP to my PC, the PC sees the hub.
is there some sort of setting i have to set in STUSB4700QTR to let my phone know that it sinks power but sources data to the hub? I have no option to program the STUSB4700QTR