Hi A power source can only propose the 5A if the cable is detected other way the source PD0 is 3A max so on source side on one CC pin you must see provided typeC current RP STD,1.5 or 3A , and on the other you must see pull down Ra from the cable fro...
Hi , STUSB4700QTR is not able to act as DRD (dual Role Data ) , it does not support any Data role swap messages , so even if you controler is device capable le link will stay hostBR
Aim of schematic is:· While stsub4500 is in explicit contract, if there is a current surge system, drop induced by surge will be absorbed by RC in order to avoid stusb4500 to disconnect due to UVLO. · During VBUS voltage ramp up, there...
Hi Yan You are true the bit 2 and 3 of the Register ALERT and ALERT_MASK are not used so you don't care about themfor each of the 4 bits of the ALERT register that are useful , you can clear it by reading 1 registerthe register bit 0 is ALERT on Phy ...