cancel
Showing results for 
Search instead for 
Did you mean: 

STSW-L9961BMS Current Lmit setting

jslee
Associate II

Hello, I'm studying the kit you provided and the stsw-l9661bms program to implement a low-capacity BMS. According to the datasheet, there are instructions to set thresholds for OverCurrent in the program. However, I couldn't find these settings in the provided Demo1~4.

 

Datasheet: VOVC_CHG_TH

 

Configuration Expected program statement: app_bms_demo.C

.CurrTh = {

.OverCurrentDischargeTh = 0, /* Over Current Discharge Threshold = 0mV /
.OverCurrentChargeTh = 0, /
Over Current Charge Threshold = 0mV /

.PersistOverCurrentTh = 0, / Persist Over Current Threshold = 0mV /

.ShockCircuitPersistTh = 0, / Short Circuit Persist Threshold = 50mV /

.ShockCircuitTh = 0, / Short Circuit Threshold = 50mV */

 

 

.OverCurrentDischargeTh , .OverCurrentChargeTh Could you please provide guidance on how to set these values if I want OCP to trigger?

0 REPLIES 0