2024-08-15 03:28 PM - last edited on 2024-08-15 11:45 PM by Peter BENSCH
Have a quick question. What is the delay time from when the EN is pulled high to when the half bridge becomes non Hi-Z? Similar is disable delay time from when the EN is pulled low? I wasn't able to find this information in the data sheet.
We will be operating in single half bridge (parallel) mode if that has any impact. Thanks!
2024-11-12 01:04 AM
Hello @twjudge and welcome to the ST Community.
Here below the typical value @ Tj = 25°C,
test conditions of Table 3 in the STSPIN958 datasheet, with "maximum slew rate" selected: