2019-01-24 01:37 PM
Hi Everyone,
I am using the STL120N4LF6AG device in a product and I was wondering if there is any have to turning it off with a negative Vgs voltage? The data sheet only lists a positive Vgs limit (40V) so it is unclear what it's tolerance to a negative voltage is.
Thanks,
David
2019-01-25 12:52 AM
Wow, 40 Volt of UGS? How think is the gate oxide? I wonder if that is a typo! For unprotected FETs, UGS is limited by the field strength, so polarity does not matter. ESD protected devices will have a diode and so will conduct current for negative UGS.
2019-01-26 05:07 PM
Agreed, It is very high, but not unheard of. I need >33V Vgs for my application, and even with an external ESD diode I am suffering from deaths. So I'm trying to eliminate possibilities, thanks for your input!