2024-11-20 2:36 PM
Hi,
The datasheets says (P173) - the VREF– s available only on UFBGA176+25 and
TFBGA240+25. When VREF- is not available, it is internally connected to VDDA and VSSA.
Our ADC input signal goes to both positive and negative.
Questions:
1. What the part number we should use, which allows VREF–? (Negative ref)
2. Is VREF– a fixed value or changeable? How is it defined relative to the input signal range?
3. Does NUCLEO-H753ZI board allow our negative ADC input signal in? If so, who is the the range (max + and max -) defined?
Thank you very much for your help,
Solved! Go to Solution.
2024-11-20 8:30 PM
2024-11-20 7:08 PM
Refer to chapter 9 Ordering information, for part number with VREF-
2024-11-20 7:12 PM
VREF+ max is Vdda (Max 3.6V), so, I suppose VREF- min is -3.6V
2024-11-20 7:17 PM
if understand correctly, NUCLEO-H753ZI board does not support negative ADC input if ADC input directly connected to STM32H753ZI pin. User may use OPAMP to shift negative input ~ positive input => 0 ~ Vdda, for example -5V ~ +5V => 0V ~ 3.3V.
2024-11-20 7:36 PM
Thanks,
“VREF+ max is Vdda (Max 3.6V), so, I suppose VREF- min is -3.6V”
What is VREF+ min ?
What is VREF- max?
Also -
Can the input signals on their selected channels of all SAR ADC be sampled synchronously under the same sampling rate?
Thanks again
2024-11-20 7:38 PM
Thanks
"Refer to chapter 9" - In which document?
Thanks again
2024-11-20 8:24 PM
datasheet
2024-11-20 8:30 PM
refer to chapter 6.3.20 of datasheet
2024-11-21 3:55 AM
The datasheets (STM32H753ZI) says (P173) - the VREF– s available only on UFBGA176+25 and
TFBGA240+25.
Should we specify it when order (STM32H753ZI)?
Thanks
2024-11-21 4:10 AM
The package type & number of pins is part of the ordering code:
https://www.st.com/resource/en/datasheet/stm32h753zi.pdf#page=348