2022-02-24 5:12 AM
I have a STPMIC1E on my board, it is used with a STM32MP157 chip.
I am currently trying to program the PMIC IC via the GUI but it won't connect to the bus. It says USB to I2C bus not connected.
Any ideas?
Thanks
2022-02-25 12:57 AM
Hi @Na.1 ,
Can you elaborate what you mean by "I am currently trying to program the PMIC IC via the GUI" ?
for STM32MP157 we usually recommand STPMIC1A or 1B .. why using a 1E ?
Are you successfully booting and executing TF-A and Uboot ?
Olivier
2022-02-25 1:55 AM
Hi Olivier
I was basically trying to reprogram the 1E chip to become a 1A by changing the register values, procedure detailed in AN5440.
I was successful in doing so, I had to use my I2C chips native interface to talk to the PMIC.
I am currently struggling with the booting, TSV flashing service failed. This occurs during the FSBL.
Yuveer