cancel
Showing results for 
Search instead for 
Did you mean: 

POWERSTEP01. Is there a way to switch cleanly between MOVE and RUN?

GoA
Associate

3 Powersteps -> 3 steppingmotors for X, Y and Z axes, voltage mode.

Is there a way to switch cleanly between MOVE and RUN commands?

Currently, when I execute RUN command after MOVE movement, motors move too slowly. Although I change the speed (target - acceleration from 0 to 1200 RPM).

MOVE alone works fine, RUN curves without MOVE also clean.

Of course I wait for SMCMD_READY, and only then I send next command with SPI.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
GoA
Associate

This was interface error . Problem solved

View solution in original post

2 REPLIES 2
GoA
Associate

This was interface error . Problem solved

Thank you for letting us know!

However, you are also welcome to post more details about the temporary misbehaviour so that other users can avoid it. Thank you!

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.