cancel
Showing results for 
Search instead for 
Did you mean: 

STPM33: UART is not responding.

RaviR
Associate

Hello,

I have design power monitor section using STPM33.

I have taken its reference from STPM33 EVK board and its datasheet.

I have attached our design schematic. Sensing the current with the shunt resisters.

Below are Test point voltages for debug:

VREF1-17 - 1.15 V

VREF2-19 - 1.15 V

VDDA-21  - 2.85 V

EN-8   - 3.30 V

VCC-23  - 3.30 V

VDDD-27  - 1.21 V

SYN-28  - 3.26 V

SCS-29  - 3.30 V

All pin status seems correct as shown above.

I am trying to read/write the registers using UART. but STPM33 is not giving any response.

There is no activity on STPM TX pin. it is always High.

I am using example code from STM for testing. Link

I also have EVALSTPM33

I had tested the STPM33 example code on this EVK with the connection of our actual MCU and with the actual UART connection shown in the attached file.

I was working fine.

I am doing the same with onboard STPM33.

MCU is sending some data on the RX line but STPM33 is not responding on TX. it is always high.

I am doubting that the STPM is not going into UART mode.

Let me know if you have other suspects where I can look?

Is there any issue with configuration and selection?

0 REPLIES 0