2013-10-15 4:48 AM
Hy, i must build a new board for control Stepper Motor. The pwm control logic and all,
is manage with new cortex STM like STM32F100RBT6B. I want an unique 3V3 logic supply for all, is possible drive and receive all the logic signal control of the L6208 or similar stepper drive controller: Clock, Reset, Half/Full, Cw ecc.. with 3V3 max high level signal ?? Naturally the Motor have separated 40 Volt high power line voltage.Thank you
Best regards2013-10-21 1:51 AM
Hi,
all the devices of the powerSPIN family are compliant with both 3V3 and 5V logic thresholds. Regards Enrico