2012-03-05 07:38 AM
STM3210E eval board has a stm32103ZG MCU on it and this MCU resides in XL-density group. The problem is related with ST motor control workbench. It has no option to generate header files for XL density devices under Control stage>MCU and clock Frequency.
Available options are :Performance line High densityPerformance line Medium densityPerformance line Low densityValue Line Medium densityValue Line Low densityHow can i generate related headers for the 103ZG MCU via motor control workbench tool.Regards.2012-03-05 11:58 PM
Hello,
you can use Performance line High density in the workbench MCU setting. Reagrds Gigi