HVLED805
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2012-01-06 1:09 AM
Hello,
I want to execute my project with HVLED805 where input voltage is 176…264 V.
Output voltage for LED equal 18 V, output current 0.45 A.
Edesign proposed the transformer with widings: Primary – 145 turns, Aux – 29 turns, Secondary – 34 Turns, transformer core EE16, Reflected voltage 80 V.
I can’t allocate these winding therefore in program VIPer Design Software v.2.24 I have counted
analogous
transformer with widings: Primary – 120 turns, Aux – 17 turns, Secondary – 20 Turns, transformer core EE16, Reflected voltage 115 V.
Edesign recommended Rsense=0.931 ohm.
For calculation of this parameter with the new transformer I have used the equation (7) of datasheet (
Off–line LED driver with primary–sensing HVLED805 -
http://www.st.com/internet/com/TECHNICAL_RESOURCES/TECHNICAL_LITERATURE/DATASHEET/CD00287280.pdf
:(
Iout=(Npri/Nsec)(Vc_led/2Rsense)
In this equation
Iout
and
Vc_led
remains invariable.
After substitution of new values
Npri/Nsec
I have received Rsense=1.31 ohm
From here I had a first question: whether correctly I have made calculations?
In advance I thank you for the answer
- Labels:
-
AC-DC Conversion
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2012-03-15 8:11 AM
Unfortunately
, this forum
is not supported
by experts
of
STMicroelectronics
.The all questions
I was able
to solve
without help.
The results
are visible
in the photo.
The device
provides
i
n the LED
current of
0.55 A
with voltage of
18volts.
The lamp
produces a
luminous flux of
1700
lumens
.
Case temperature
is 52degrees
Celsius.
Heat sink
of LEDs has temperature
55
degrees Celsius.
It's all right
.
________________ Attachments : P1010008.jpg : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Htzj&d=%2Fa%2F0X0000000ab8%2FeaQZkcCS2ggGt83Fn2pVEeynMAFYEY9f.fKbjdxZEg0&asPdf=false