2020-09-29 6:01 AM
Can I connect oscillograph to Steval -SPIN3201 for measurement currents of the phase? Where is this point on board?
Solved! Go to Solution.
2020-09-29 11:28 PM
Yes, of course.
Please take a look at the circuit diagrams and the UM2154 user manual of the STEVAL-SPIN3201. Perhaps you will find the shunt connections SENSE1P, SENSE2P and SENSE3P, which are amplified and then fed into the control at PA3/4/5. And if you then look at the board, you will find these test pads with a metal ring and the label PA3/4/5 around the controller.
Does it answer your question?
/Peter
2020-09-29 11:28 PM
Yes, of course.
Please take a look at the circuit diagrams and the UM2154 user manual of the STEVAL-SPIN3201. Perhaps you will find the shunt connections SENSE1P, SENSE2P and SENSE3P, which are amplified and then fed into the control at PA3/4/5. And if you then look at the board, you will find these test pads with a metal ring and the label PA3/4/5 around the controller.
Does it answer your question?
/Peter
2020-09-30 10:43 AM
How I can use STEVAL-SPIN3201 for BLDC with MotorControl Workbench? In MotorControl Workbench only two types motors? To choose SM PMSM?
2020-10-01 5:15 AM
Hello @oleg_sidorovich_1981
please if @Peter BENSCH answered your main question "Select as Best" his reply.
Moreover, to help the Community to easily find the answer to similar questions open a new topic with the second request.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.