2024-06-30 06:31 AM
Dear ST:
Why I can not discharge my battery? Only Charge into it?
my setting are below:
1、Hardware:CN2 connector:I connect a load(small DC fan,or a resistor)to CH+ CH-;
2、Software:In GUI, I run file ( Current Acquistion Init - CC+CSA.csv),
Activate fuse, Charge ON, Discharge ON;
but my battery did not discharge at all ?
the attached file is my Demo details, Thanks !
2024-06-30 06:57 AM
I want to add more information:
I can use GUI to charge my battery , and the current usually 30~50mA;
but I can not use Tera term, there is no current flow in Tera term;
Wish this can help !
2024-07-07 03:23 AM
Dear ST:
Finally ,I found the fuse (ITV4030L2015NR)was broken, that was why I can not charge and discharge my battery !
I short circuit (bypass)the fuse ,and all works well now;
I use a DC24V power source, and my charging current is about 1.2A(1200mA);
hope this can help !