cancel
Showing results for 
Search instead for 
Did you mean: 

Spice model for STB60NF06 mosfet

Herwig
Associate

Hi,

I am looking for a spice model for this mosfet (preferably one that runs stable in LTSpice).

Purpose is to do some simulations for a SMPS (detailed calculation during transients should be supported by the model).

I did not find in STB60NF06 - N-Channel 60V - 0.014Ohm - 60A - D2APK StripFET(TM) II POWER MOSFET - STMicroelectronics

(For some mosfets, it is available at this place).

Is a model for this mosfet available?

Herwig.

 

1 ACCEPTED SOLUTION

Accepted Solutions
AScha.3
Super User

The AI says :

 

STB60NF06 spice model

 

The STB60NF06 is a N-Channel 60V - 0.014 Ohm - 60A DPAK STripFET II MOSFET from STMicroelectronics. The spice model for this device is not explicitly provided in the search results. However, the device’s datasheet can be used to create a spice model.

Device Parameters

  • Maximum Power Dissipation (Pd): 110 W
  • Maximum Drain-Source Voltage (Vds): 60 V
  • Maximum Gate-Source Voltage (Vgs): 20 V
  • Maximum Gate-Threshold Voltage (Vgs(th)): 4 V
  • Maximum Drain Current (Id): 60 A
  • Maximum Junction Temperature (Tj): 175 °C
  • Total Gate Charge (Qg): 49 nC
  • Rise Time (tr): 108 nS
  • Drain-Source Capacitance (Cd): 360 pF
  • Maximum Drain-Source On-State Resistance (Rds): 0.016 Ohm

Note

The spice model for the STB60NF06 can be created using the device’s parameters and characteristics. However, the exact spice model is not provided in the search results.

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

3 REPLIES 3
Peter BENSCH
ST Employee

Welcome @Herwig, to the community!

The MOSFET was launched in 2004, when spice models were still rarely available. I fear that no more models will be created for such an old device.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
AScha.3
Super User

The AI says :

 

STB60NF06 spice model

 

The STB60NF06 is a N-Channel 60V - 0.014 Ohm - 60A DPAK STripFET II MOSFET from STMicroelectronics. The spice model for this device is not explicitly provided in the search results. However, the device’s datasheet can be used to create a spice model.

Device Parameters

  • Maximum Power Dissipation (Pd): 110 W
  • Maximum Drain-Source Voltage (Vds): 60 V
  • Maximum Gate-Source Voltage (Vgs): 20 V
  • Maximum Gate-Threshold Voltage (Vgs(th)): 4 V
  • Maximum Drain Current (Id): 60 A
  • Maximum Junction Temperature (Tj): 175 °C
  • Total Gate Charge (Qg): 49 nC
  • Rise Time (tr): 108 nS
  • Drain-Source Capacitance (Cd): 360 pF
  • Maximum Drain-Source On-State Resistance (Rds): 0.016 Ohm

Note

The spice model for the STB60NF06 can be created using the device’s parameters and characteristics. However, the exact spice model is not provided in the search results.

If you feel a post has answered your question, please click "Accept as Solution".
Herwig
Associate

Ok.

Thanks for the feedback.